3/5/2018 8:06 PM | |
Joined: 6/5/2009 Last visit: 3/18/2025 Posts: 153 Rating:
|
Dear All, Attached are 2 pictures depicting the system architecture on the PROFIBUS level of communication with the ET200M I/O's and the other consists of MODBUS TCP system. Is it feasible to have multiple MODBUS TCP servers on redundant basis with a redundant S7-400 H station? If so is there any example to describe the connection and the program. Regards, Grim Reaper AttachmentSystem Architecture.zip (64 Downloads) |
Last edited by: Grim Reaper at: 3/5/2018 8:09:41 PM |
|
Follow us on