Industry Online Support
Technical Forum
9/22/2012 8:19 AM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dear elake, thank you for your quick response. 1. Its customer requirement that they want to swap the plc; why ,am not sure. But we have to provide the solution. 2. Anybody can post a simple sample program/link for H -CPU. I made hardware configuration, but not tested so far . In plc program, need to use any additional blocks? Can we do the program using the address of Master Plc's IOs? We are using some special type of hardware and connector(field interface module), so that we can connect 4-20ma also.FIND ATTACHMENT 4 DETAILS
AttachmentUL08AI (RED)-D25-SPD FOR 6ES7-331-7KF02.pdf (148 Downloads) |
|
|