Industry Online Support
Technical Forum
7/14/2013 10:13 PM | |
Posts: 378 Rating: (73) |
Hello sankannan, This is taken from LOGO Soft comfort v7 Help manual of weekly timer: The internal real-time clock of LOGO! is buffered against power failure. The buffering time is influenced by the ambient temperature, and is typically 20 days (for LOGO! 0BA7 devices) or 80 hours (for LOGO! 0BA6 devices) at an ambient temperature of 25°C. The LOGO! 0BA6 devices and higher support the option of a battery card or a combined program module (memory) and battery card. The real-time clock is buffered for several years with either of these cards. Hope helps, |
7/15/2013 5:58 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating: (709) |
Hi sankannan, you can mount the memory and backup battery 6ED1 056 7DA00 0BA0. |
Follow us on