Industry Online Support
Technical Forum
12/19/2011 5:47 AM | |
Posts: 2964 Rating:
|
Hello.... Check this.... 3RK2400-1FQ03-0AA3 AS-INTERFACE COMPACT MOD. K60, DIGITAL, 4I/3O, IP67, 4 X 1 INPUT, 200MA MAX., PNP 3 X 1 OUTPUT, 2A, DC 24V 4 X M12 STANDARD SOCKET 4 X M12 SOCKET M. Y-II ASSIGNM. technical details attached in the link.... http://support.automation.siemens.com/WW/view/en/22430746/td manuals link attached... https://support.automation.siemens.com/WW/llisapi.dll?query=3RK2400-1FQ03-0AA3&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW Regards, Prakash |
This contribution was helpful to
1 thankful Users |
12/19/2011 10:37 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating:
|
Sir, Thanks for your document, If i need any more information , i come back. |
Regards, |
|
Follow us on