5/17/2009 6:52 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating:
|
HI all.... How tomodify the program for CP341 modbus masterfor connecting2 slaves(energy meters)? The example program was suitable to only one slave. I also tried for obtaining the communication of those 2 slaves and i obtained the values. But the problem was i am facing delay while obtaining the values and i tried to reduce the delay but the values are overlapping in b/w the corresponding DBs. I also attach the program what i used plz check the program. In the attached program i used the FC20 for meter looping. I am moving the corresponding DB.N0 to MW160 addr which is used in FC23 Those who are all know the solution kindly help me to solve this.... Thanks in advance.... AttachmentzXX21_04.zip (250 Downloads) |
All is well :-) |
|
5/20/2009 8:22 AM | |
Posts: 12 Rating:
|
Hi Sam, It would be works, Regards, Sora |
6/9/2009 5:28 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating:
|
Hi... |
All is well :-) |
|
Follow us on