11/29/2022 11:44 PM | |
Joined: 9/27/2006 Last visit: 1/30/2023 Posts: 11948 Rating:
|
Hello Carbondale; Maybe a little documentation on the S7-1200 can help you out, have a look at the S7-1200 System Manual: https://support.industry.siemens.com/cs/ca/en/view/91696622 In the screenshot below, taken from that manual, you will find that you (the programmer) select the start address of every signal module attached to the CPU rack. The image shows you in which screenyou can do that, and how to retrieve the start address of any module, whether it was assigned manually (by the programmer) or automatically by the hardware configuration, upon creation of the signal module. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/30/2022 13:47:55 |
|
11/30/2022 8:23 AM | |
Joined: 6/19/2017 Last visit: 1/27/2023 Posts: 6401 Rating:
|
Hello Carbondale, please attach your files as an attachment and don't use ibb as a filesharing hoster. I can't open and check it, because the website is blocked. If you want to attach more than one file, you can create a zip file to attach more than one file. Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to
1 thankful Users |
Follow us on