4/29/2020 1:12 PM | |
Joined: 9/21/2010 Last visit: 1/7/2022 Posts: 7 Rating: (0) |
Hi, Found a topic regarding similar problems. I have a the application where V20 runs a motor of the hammer. Motor is attached over the belt with driving wheel of the hammer. I have a problem with regenarative mode. It trips to F2 when stopping. I have extend the ramp-down time and then there is no F2 fault. But the application demands shorter ramp-down time so I decided to order breaking module and breaking resistor. I configured it via Sinamics configurator for my V20 2,2 kW - 6SL3210-5BE22-2UV0
I looked the Sinamics V20 manual regarding wiring and that is clear. You suggested to disable V_dc_max controller ? Is that ok? Is there any other parameter to be changed expect ramp-down time which should be reduced? What is the recommendation for adjusting Duty cycle control knob on breaking module?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2020 07:32:54New subject after splitting |
|
Follow us on