6/11/2015 8:13 AM | |
Joined: 11/8/2011 Last visit: 3/18/2025 Posts: 92 Rating:
|
Hi! I have a project in Step 7 v13 SP1 with S7-1211C CPU (6ES7211-1BE40-0XB0 v4.1) and CM 1241 (6ES7241-1CH32-0XB0 V2.1). I need to read in the 20001 - 29999 interval. The problem is that this interval appears not to be defined in standard Modbus RTU. In the Modbus_Master function help from Step7 v13 SP1 I read that if I use MODE 104 I can read registers form 0 to 65535. MODE uses FC04 for reading. I found a recent FAQ from Siemens referring to MODE 104, but not explicitly to 20001 - 29999. My querstion is if someone read in 20001 - 29999 interval in this way. Unfortunately I cannot test this because I do not have access to the slave with which I am supposed to communicate until commissioning. Best regards, h2_504 |
Follow us on