Industry Online Support
Technical Forum
11/7/2011 12:29 PM | |
Posts: 3037 Rating:
|
Hello, What you want change in the registry? The function "regedit" does not work on the panel. It is not the complete version of WinCE on the panel. Tweety |
1/10/2012 3:38 PM | |
Posts: 5 Rating:
|
Thanks, Where can I get the runtime you mention?
|
1/11/2012 4:07 PM | |
Posts: 3037 Rating:
|
Hello, you should ask your siemens sales for the runtime of WinCC V11. ---> siemens sales Tweety |
7/2/2013 3:33 PM | |
Posts: 4 Rating:
|
Hi Everybody I found something, but please do not do what I will write here, because you can loose the guarantee!!! Do not download the Windows Compact Framework 2.0 from here: http://www.microsoft.com/en-us/download/confirmation.aspx?id=22808 After that, do not install this on your desktop computer After that, do not copy this file to a pendrive (memory stick) C:\Program Files\Microsoft.NET\SDK\CompactFramework\v2.0\WindowsCE\wce500\x86\NETCFv2.wce5.x86.cab C:\Program Files\Microsoft.NET\SDK\CompactFramework\v2.0\WindowsCE\wce500\armv4i\NETCFv2.wce5.armv4i.cab First one is the install file for Compact Framework 2.0 for x86 processors, second one is for ARM processors. Copy only the one is matching with your processor. After that, do not copy the CAB file to your panel from the pendrive (memory stick) After that, do not start the copied program, and do not install it. After that do not download the Simple Little Registry Editor from this URL: http://www.eurotech-inc.com/Wince-code/RegEdit.asp After that do not copy it to the panel and do not run. If you came to this point, even if I said do not do, then please close the regedit program now, and do not modify anything. |
Follow us on