5/24/2023 3:08 PM | |
Joined: 4/6/2022 Last visit: 5/24/2023 Posts: 1 Rating: (0) |
Hi everyone! I'm attempting to setup an HMI system with validated remote control through Sm@rtserver, as described in this document. I'm running into a very strange issue where the keyboard is not displayed properly on input. Here is a link to a short YouTube video showing this behavior. When I use the Remote HMI to input text, the keyboard shows on the local HMI, but input here is still not allowed. On the Remote HMI, there is a screen saying that input is disallowed, while input is allowed and shows up on the local HMI. Very strange! This issue only appears to be occurring when the 'No local input during client sessions' setting is enabled in the WinCC Internet Settings (in the control panel). If this setting is disabled the keyboard will function normally. However, we need to block local input for this system to meet Customer specification. Is there something about this setting that is known to cause issues? What else can I check to correct this behavior? Thanks in advance for your help! Some information about this project: Software version: TIA Portal V14 SP1 Update 5 WinCC version: WinCC Advanced V14 SP1 Update 5 Panel version: TP700 Comfort (article no. 6AV2 124-0GC01-0AX0, version 14.0.1.0) |
Last edited by: Jen_Moderator at: 05/25/2023 07:44:19Link optimized. Text formatting optimized. |
|