6/8/2011 5:16 AM | |
Posts: 30 Rating: (0) |
Dear Sandman sir, this same problem also with me,but my HMI is MP277 10'' Touch. It is password protected so we cant entered in control panel, now i want to reset it. my ques. is >> which cable i have to used, it supports RS232/LAN my first choice is LAN. and how can i know the settings(baud rate in case of RS232, ethernet is select or not). plz help me. thnks naveen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/16/2018 9:11:29 AMNew subject after splitting |
|
6/8/2011 10:54 AM | |
Posts: 30 Rating: (0) |
Dear Sir, this FAQ is very useful, but it still required IP address on MP , so how can i configure it without enter in control panel because we dont know its password. thnks naveen AttachmentMP rqurd IP add.zip (349 Downloads) |
3/16/2018 9:15 AM | |
Joined: 6/19/2017 Last visit: 5/27/2024 Posts: 8079 Rating: (165) |
New question published by Mr. Pintu is split to a separate thread with the subject IP address of OP 377 19". Best regards |
My Forum is the place to personalize your profile, |
|