9/25/2016 3:13 PM | ||
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello, perhaps it refers to this: |
|
This contribution was helpful to1 thankful Users |
9/25/2016 11:13 PM | |
Posts: 116 Rating: (2) |
Hello Ste39, Thanks for your reply. But I need more explaination about my questions. 1-
How can we check this point in the program for Ethernet,Profinet,Profibus,.......communication? 2-
Please explain this point? 3-Kindly check the following result: We can replace the inverter to another brand without modifying PLC program if: No device ID and No vendor ID in the PLC program and the telegram is similar. Best regards..... |
9/29/2016 7:04 AM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22213 Rating: (2979) |
Hello, the check for Vendor/Device ID is in the FW of the PLC, you can't disable such feature because is FW and not USEr PLC Program.
Christoph |
This contribution was helpful to1 thankful Users |
Follow us on