2/14/2013 12:48 PM | |
Joined: 10/11/2006 Last visit: 4/24/2025 Posts: 5989 Rating:
|
Hello, Please descripe the functionality of the axis, for example only positioning, or gear synchronisim to an external encoder, or electronic cam to an external encoder, print mark correction ... Do you know the peak current in your application and the rated current in your application (you can do a MASTERDRIVES trace of the current and max. load cycle)? The best is to choose the components with SIZER, so the additional components, like SMC20 could be choosen there: |
With best regards, |
|
Follow us on