2/4/2014 4:19 PM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Hello, Yes if the CPU is the same, it's that simple. Both hardware config and Program are stored on the MMC. If the CPU is not the same the CPU will ask for an overall reset. How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? Please note that all M-memory and DB's are setback to it's initial state, so if there are i.e.any machine settings changed in the old CPU the settings will be setback to it's Original state. Regards, Marcjan |
Problem solved? |
|
2/4/2014 4:53 PM | |
Posts: 9 Rating:
|
Hello Marcjan Thanks for the quick reply. Very helpful information. |
Follow us on