11/2/2017 10:24 AM | |
Joined: 6/1/2015 Last visit: 10/14/2024 Posts: 11 Rating:
|
And the second attachment.. |
11/2/2017 5:50 PM | |
Joined: 6/1/2015 Last visit: 10/14/2024 Posts: 11 Rating:
|
I think i solved the problem. After some more digging through the forums I've found a thread about the same problem I was having. Link for the original thread is here https://support.industry.siemens.com/tf/ww/en/posts/controller-alarms/177978/?page=0&pageSize=10 The tags I thought were giving the problem were indeed the right ones. So by recreating the connection between RT and device proxy the software generated the missing tags and after that the program compiled succesfully. The tags created are of the datatype RAW. Tags are generated to the default tag table under "System tags". They are named RDT_RawDataLog and RDT_RawEvent, from which the RDT_RawEvent is the one used by the controller alarms both for protocol tag and akcnowledgement. Case closed, hope this can be of some help if someone stumbles to the same issue again in the future. Cheers! -L |
This contribution was helpful to
1 thankful Users |
Follow us on