11/13/2015 6:06 PM | |
Posts: 6 Rating:
|
Hello! I am trying to make a request to the slave using modbusRTU(RS485) S7-1200 -> ET200SP -> CM_PtP(master) -> ModiconM221(slave). In the handbook recommended use MB_COMM_LOAD and MB_MASTER. When the function MB_KOMM_LOAD is called it occurs error and the status = 16#8180. Why such an error can occur, and what can I do to successfully read information from the slave device? AttachmentCM_PtP- Modicon RS485.zip (89 Downloads) |
Last edited by: Gleb78 at: 11/13/2015 6:09:26 PM |
|
Follow us on