12/15/2020 4:21 PM | |
Joined: 10/11/2006 Last visit: 3/26/2025 Posts: 6000 Rating:
|
Hello, there only the possibilities mentioned in manual. 3.11.12 Resetting the "Homed" status (S7-1500, S7-1500T) https://support.industry.siemens.com/cs/ww/en/view/109766462 Absolute encoder In the following cases, the "Homed" status is reset, and the technology object must be rehomed. ● Replacement of the CPU ● Modification of the encoder configuration ● Restoration of the CPU factory settings ● Transfer of a different project into the controller When you use a new absolute value encoder you need to home the absolute encoder once again. Resetting the memory of the CPU or upgrading a project does not require another absolute value adjustment. Maybe it is possible to configure "incremental encoder" when you deactivate "Automatic Dataexchange" for encoder. |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
Follow us on