4/16/2018 5:10 PM | |
Joined: 2/17/2012 Last visit: 4/14/2025 Posts: 21 Rating:
|
Hello, I am trying the same thing - reset the Min and Max values of a PAC4200 with WinCC Professional but with no success. Has someone succeeded in doing that? In the manual it was said that you should use these registers (pic2):
60002 1 Reset maximum values Unsigned short 0x06 When I enter the addresses like shown in pic1 the tag field goes offline (pic3). I tried a lot of things in the configuration but it did not go well. Has anyone done that? Best Regards, Sv.Veselinov ------------------------------------------------------------------------------------------ Attachmentpac.zip (43 Downloads) |
Last edited by: Jen_Moderator at: 4/17/2018 10:40:33 AMNew subject after splitting |
|
Follow us on