12/12/2018 11:33 AM | |
Joined: 12/18/2014 Last visit: 12/3/2023 Posts: 31538 Rating:
|
Use mathematic instruction. If you enter the value via display, the value would be saved in a flash Memory. |
12/12/2018 11:49 AM | |
Joined: 12/18/2014 Last visit: 12/3/2023 Posts: 31538 Rating:
|
I must just go out of office. Later i will give you an example. |
12/12/2018 12:08 PM | |
Joined: 7/24/2017 Last visit: 12/1/2023 Posts: 8 Rating:
|
Thank you. I'm waiting your solution. |
12/12/2018 3:58 PM | |
Joined: 7/24/2017 Last visit: 12/1/2023 Posts: 8 Rating:
|
No. The set temperature will be between +10 and +30. |
12/12/2018 4:12 PM | |
Joined: 12/18/2014 Last visit: 12/3/2023 Posts: 31538 Rating:
|
In the attachment a possible solution. The setpoint from the HMI (or App) is polled to see if it is opposite the last stored setpoint. If so, then the current setpoint is stored. AttachmentStoring_Setpoint_from_HMI_Fail-safe_in_LOGO!_(automatically)_FS4.zip (582 Downloads) |
Follow us on