12/23/2019 5:42 PM | |
Posts: 17 Rating: (0) |
Hi Dear Experts! I am doing a project to control Air conditioning and would like if correct program to work with 2 ar conditioning and also doing the control of temperature with PT100 connected on module AM2 RTD, please note bellow: 1 - Two air conditioning connected in output Q1 and Q2 (only power on and off) 2 - Two PT100 both connected in AM2 RTD(AI1 and AI2) Air conditioning 1 should work 12hr directly, but if temperature more than 24C should power on Air conditioning 2 and shutdown if temperature 22C. Both should work like this, otherwise after 12hr Air conditioning 2 should work 12hr and if termperature room more than 24C should power on Air conditioning 1 and less than 22C come power off. Anyone can review te program to me and if ok and give me feedbak? I´m so sorry I´m not expert for this, but I gave this solution to my company to reduce light consumption and after tests we will apply more than 100 devices Logo in our project. AttachmentTest Temperature.zip (286 Downloads) |
12/23/2019 6:17 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
I'm not sure I understood you correctly. Maybe that's what you mean. AttachmentTest Temperature_V2.zip (324 Downloads) |
12/23/2019 7:13 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
So like this?
AttachmentTest Temperature_V3.zip (339 Downloads) |
12/23/2019 7:30 PM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33113 Rating: (4088)
|
I wish you the same .... |