6/21/2022 4:44 AM | |
Joined: 8/25/2021 Last visit: 7/15/2022 Posts: 11 Rating:
|
Hi bergmanu, [snip] Another question: I have configured my IoT 2050 adv well with Example Image v1.0.2. Now I would like to rewrite the sd card with v1.2.2. Should I directly rewrite it and access IoT with previous user/passwords? Or must I re-configure the Industries OS and then access the Example Image?(because the eth0/eth1 in v1.0.2 refers to P2/P1 respectively, but in v1.2.2 oppositely. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/21/2022 06:33:09New subject after splitting Last edited by: Jen_Moderator at: 06/21/2022 06:33:52Division of question into separate topics. |
|
Follow us on