Industry Online Support
Technical Forum
2/12/2013 9:54 AM | |
Posts: 391 Rating: (50)
|
Hello, basically you need some software that transfers the tool data from NC memory to RFID chip and vice versa. Siemens has a product that helps to implement this task, named TDI Ident Connection. It transfers tool data between NC and a configured DB in the PLC. Then you need to write your own PLC code to transfer tool data between this DBand the RFID reader/writer, which is usually connected to the machine via Profibus or Serial interface RS-232. TDI Ident connectionintegrates itself in the HMI-Advanced and can be configuredvia.ini files. A prerequisite is Tool Management functionality (tool magazines instead of the simple tool list) on the 840D. Here is a link to the manual http://support.automation.siemens.com/WW/view/en/28733140 Of course there are also third party products andsome manufacturers of RFID systems for machine tools offer their own software for SINUMERIK. |
This contribution was helpful to1 thankful Users |
Follow us on