11/24/2015 5:38 PM | |
Joined: 10/16/2014 Last visit: 9/14/2022 Posts: 2 Rating: (0) |
Thank you Maestro |
11/25/2015 10:50 AM | |
Joined: 4/3/2008 Last visit: 4/22/2024 Posts: 385 Rating: (16) |
Oguz, you are welcome. The example is available also in the following zip file. DVD3\Utilities_Applications\src\Examples\ProgrammingExamples\D425\E_PIB032.zip pigroplc |
This contribution was helpful to1 thankful Users |
9/19/2019 8:31 AM | |
Joined: 4/11/2015 Last visit: 4/16/2024 Posts: 12 Rating: (0) |
What is the communication protocol between your RFID and 1SI module?For example the modbus RTU. |