1/19/2022 3:34 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello ferox1338, I am not aware of any problems with the firmware update. However, there is no such thing as 100% security. The CPU must be compatible for the firmware update. I would also save the data on a separate MMC beforehand. The following entry describes the requirements and the procedure for the firmware update of the S7-1500 CPU: Description of Firmware Update for S7-1500 CPU, Displays, ET 200SP CPUs und ET 200pro CPUs With best regards |
Follow us on