7/14/2022 10:23 PM | |
Joined: 5/23/2022 Last visit: 9/25/2022 Posts: 39 Rating:
|
Hello please help; I want to replace Masterdrive VC with sinamics G120 and I try to take the parameter from Masterdrive VC and find the equivalent parameters in sinamics G120 and there is some parameter I didn't understand in drive monitor: I want to know why "n/f (act)" which is speed frequency actual value is interconnected with Binnector parameter P232 (Src n/f RegAdapt) ; the description of parameter P232 is : BICO parameter for selecting the connector from which the input signal for the gain adaption of the speed controller (P235) is to be read in. Precondition: P100= 0, 3, 4, 5 (v/f control with n control, vector control types) Function diagrams: 360.3, 361.3, 362.3, 363.3 more detail shown in attached image |
Follow us on