7/8/2019 11:15 AM | |
Joined: 9/9/2012 Last visit: 2/5/2025 Posts: 48 Rating:
|
Hello I have a rolling door similar to this one to be controlled with a G120c and S7 15152PN and a PROFINET encoder I want to control the door in position, but my doubt is when I configure the linear movement done by load per motor revolution leadscrew, that in the case of a rolling door will vary if the door is completely unwinded or not. Because if the door is up (opened), a motor revolution will unwind more door material than at the end of movement, that's my feeling. right? Will be necessary to know the thickness of the door material and calculate how much grow the diameter in each turn? This in the case that I use a "TO positioning axis", and what about "speed axis"? What option will be best? There is any Siemens application for this? Thanks in advance to all the community.. AttachmentFigures.zip (92 Downloads) |
Last edited by: culebrasx at: 07/08/2019 14:47:51Last edited by: Jen_Moderator at: 07/09/2019 09:56:28Removed links and added files as an attachment. There are 10 types of people in this world, those who understand binary and those who dont. |
|
7/9/2019 8:44 AM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating:
|
Hello, |
With best regards, |
|
Follow us on