7/20/2018 6:54 AM | |
Posts: 1283 Rating:
|
Hi All, Just few questions about my testing. 1) I tried TCON, TRCV, instructions, but I received some characters which i get using TELNET cmd window which is not the actual data. I understand because through TElnet cmd i didn't use any addressing or anything. so it is fine. 2) I tried MODscan software with remote telnet server and with proper addressing, it can read data from the meter. So I think there is no problem in communication. 3) then i tried MB client instruction with PLC tio see whether i can have any luck. I know i am doing something which is not right, because there is no conversion from MB RTU to MB TCP. so MB client with TCP can't work. My question is that how can i achieve the same what Modscan software did by using the S7-1200 PLC. what instructions should I use? Can someone give a sample program for this so that i put it in my PLC to see the function. I had attached the Data in the attachment. Please have a look and guide me. If I can make this work, it will save me sometime instead of buying any extra Modbus converters or Communication modules in the project. and it will be a good learning for me as well. Thanks, Jay AttachmentMB.pdf (251 Downloads) |
Last edited by: Jay. at: 7/20/2018 7:16:13 AMchanged attachment file format to PDF for easy viewing |
|
Follow us on