12/24/2012 1:17 AM | |
Posts: 2 Rating:
|
Good Evening I need some help, text may not be as readable as I am using the translator. I need to program a PLC to make reading a central fire have a PLC with S71200 CM1241 RS485 connection to the center where she has a protocol converter modbus rtu slave, so my connection will be central to the PLC 485 rs will stand as master and depending on a range of smoke detectors and glass break will trigger a certain output of electromagnets that triggered PLC and shut some doors, also will have a supervisory monitoring ellipse E3 with a map of the plant where the sensors are. my doubts as to the right configuration for the PLC to read the plant. en annex the allocation of the central points. Why can help me thank.
AttachmentAlocação_dos_pontos_da_Central_de_Alarme_de_Incendio.pdf (552 Downloads) |
12/27/2012 3:33 PM | |
Posts: 3093 Rating:
|
Hello Cladibohn, yes, your configuration sounds good. Regards, Kaulquappe |
1/1/2013 6:20 PM | |
Posts: 2 Rating:
|
Could someone help me on the question of PLC programming for correct reading of the central? |
1/2/2013 4:04 PM | |
Posts: 3093 Rating:
|
Hello Cladibohn, our friendAutomatizzando published a Modbus sample. Regards, Kaulquappe |
Follow us on