7/21/2023 3:37 PM | |
Joined: 1/12/2023 Last visit: 2/6/2025 Posts: 2 Rating:
|
Hello dear TIA community, My Runtime freezes for about 30-60seconds when a user is changed (so when a different user than the actual user is logging in via the popup, or Logout is pressed, but not at re-login of the same user). This screen contains 170 alarm-control elements and it only needs to be open in the background. The only purpose of it is to provide alarm counts based on 170 filters, which can then be read by my vbscript by reading out the „List“ count from the statusbar of those 170 alarm-control elements. AttachmentRT freezes.zip (275 Downloads) |
Follow us on