9/29/2015 9:47 AM | |
Posts: 9 Rating:
|
Hi, I have a problem with the correct operation of faceplate. I created some faceplates. Put them onto screen and connect interface properties. After I start simulation on my laptop everything works fine, all faceplates work correctly. When I download project to system file and transfer it to PC (where the RT Professional is installed ), after running RT all created faceplates are not working propertly (all elements of faceplate are displayed irrespective of signals from the PLC). Does anyone know what could be the reason for such behavior? -------------------- Software: STEP7 V5.5 + SP4 WinCC Professional V13 + SP1 Update 3 WinCC Runtime Professional V13 + Update 3 Hardware: S7-317-2 PN/DP Thank you.
1. Facplate view - splt elements 2. Project view - complete faceplate 3. RT view 4. Simulation view AttachmentDifferent_views.zip (119 Downloads) |
Last edited by: maqu at: 9/29/2015 9:48:19 AMLast edited by: maqu at: 9/29/2015 9:49:41 AMLast edited by: Min_Moderator at: 9/29/2015 4:06:40 PMAdd attachment |
|
9/29/2015 4:13 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
I recommend installing Update 5 of WinCC V13 SP1. Could be one of the bugs that got fixed. Did you use the computer name of the RT PC (OS) in the device configuration? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
10/6/2015 3:35 PM | |
Posts: 9 Rating:
|
Update 5 installation didn't help. Any other idea? |
10/20/2015 11:14 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello did you try the WinCC Channel Diagnostics Tool? WinCC Professional manual chapter: |
Last edited by: H.J. at: 10/20/2015 3:17:05 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on