9/25/2019 12:04 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
Hi, either you go to the mask of the communication receive direction and connect the words 3 and 4 (for example) from here to p1138 and p1139. Or you go to the mask of ramp function generator to p1138 and p1139 and here select as source r2050[x]. "X" stands for the word -> e.g. r2050[2] is PZD word 3. This is how the BiCo system works in SINAMICS drives. There is a so called source (Binektor outputs or connector outputs) and a so called sink (binektor inputs or connector inputs). You can either go to the sink (e.g. p1138) and connect the source (e.g. r2050[x]) or vice versa. Attached see my screenshots for Starter and TIA (I guess you use Starter for your G120C commissioning). AttachmentStarter_TIA.zip (128 Downloads) |
Best regards, |
|
Follow us on