2/20/2012 10:46 AM | |
Joined: 11/28/2011 Last visit: 1/22/2025 Posts: 53 Rating:
|
Dear Support I detect one problem just I hope you can help me, When I switch power on on the Siemens CPU then the all communication is starting but on the end Run flashing 2hz and data transfer not running. And the CPU in HW config is gray and I can not look to Diagnostic buffer :( when I disconnected cable from the master CPU and again connected then is running. So I must do every time plug on and off connector which is connected to master CPU. Thank you very much . AttachmentDiagnose.zip (55 Downloads) |
Last edited by: MartinChyska at: 2/23/2012 6:53 PMLast edited by: O_Moderator at: 2/20/2012 11:36 AMnew subject after splitting from /tf/WW/en/Posts/69297#top |
|
2/27/2012 11:53 AM | |
Posts: 1547 Rating:
|
Hello, have you loaded the requestet error OBs (OB83,OB85,OB86)? |
Follow us on