12/1/2017 3:59 PM | |
Joined: 3/27/2009 Last visit: 8/7/2023 Posts: 92 Rating:
|
I found one problem, in my last program i am using the running hour timers. During testing i make several minor adjustments and evry time that i upload the software (V8.1) asks if i want to reset the timers. If i select YES the timers are reset and if i select NO then the update is not loaded .... The not uploading of any program"" change when i also want to keep the timers is strange or do i make a mistake ......... Any help is usefull I include my program , i did not clean it out yet .. sorry about that. the function is a little complicated but i need it to work on several setups.... Attachmentcylinder oil shifting pump control.zip (43 Downloads) |
Follow us on