12/11/2006 2:46 PM | |
Posts: 4 Rating:
|
There are twoWinCC machines currently running the HMI applications on site, so that part of the system is take care of. We also have Dat@Monitor / Webnavigator on our machine. How do we configure the WebNavigator portion to handle the 2 different applications. We have only been able to configure 1 web interface ata time. Where is the web configuration stored in this situation. |
12/11/2006 3:50 PM | |
Posts: 4 Rating:
|
There are 2 existing WinCC machines running currently in the field. We have a new pc that can be a client to the existing WinCC applications and also can run the Dat@Monitor / WebNavigator software. We need to be able to have a readonly view of the 2 WinCC apps screens, thus the need for the Dat@Monitor / WebNavigator portion. Per your previous post "Thethird one is configured as a Client With Project and accesses the data from the two servers. You then install WebNavigator on the client machine. This gives you access to both projects data from a webnavigator client." it sounded as though we could use WebNavigator to view both projects screens on our new client machine. Any further assistance is greatly appreciated! |
Follow us on