1/4/2024 8:29 AM | |
Joined: 2/17/2020 Last visit: 4/16/2025 Posts: 1250 Rating:
|
Hi, As detailed in the WinCC V18 (TIA Portal) delivery release note, for this new version:
So, you would need to install RT Advanced V17 and have a RT Advanced V17 (also valid for V18) license. |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
1/4/2024 9:07 AM | |
Joined: 5/30/2022 Last visit: 4/16/2025 Posts: 634 Rating:
|
Hi Roby, There is no download link for WinCC RT Advanced V18, as WinCC RT Advanced V18 does not exist. WinCC RT Advanced will continue to be configured with device version V17.0.0.0 in V18. The project therefore runs on WinCC RT Advanced V17 after the transfer on a PC/IPC. The installation data carrier for WinCC RT Advanced V17 can be downloaded from the support pages at the following link: SIMATIC WinCC V17 Runtime (TIA Portal) The licence can be found in the following Excel: AttachmentWinCC_V18_MLFB_List (3).xlsx (242 Downloads) |
Last edited by: Jen_Moderator at: 01/04/2024 11:27:00Text formatting optimized. If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
Follow us on