12/1/2017 10:28 AM | |
Posts: 5 Rating: (0) |
I allready have components on Profibus and on Profinet, and I dont have extra "contacts" if I also should create a Modbus TCP network (or Modbus RTU). |
12/1/2017 10:32 AM | |||
Posts: 5 Rating: (0) |
I have now recieved a GSD-file from "device supplier". Unfortunately, it did not appear to be installable. I hope I will receive a better one soon. :-)
|
||
12/1/2017 3:03 PM | |
Joined: 7/7/2010 Last visit: 3/28/2024 Posts: 14520 Rating: (2331) |
Please explain what happens when you attempt to add the GSD to your project? What version of TIA Portal are you using, and what PLC?
|
science guy |
|
12/4/2017 9:58 AM | |
Posts: 5 Rating: (0) |
They asked me to rename the GSD file to concube.gsd instead of Profibus_8.gsd. Then it worked. Strange, but nice to have an istallable file.
|
This contribution was helpful to1 thankful Users |
Follow us on