10/18/2016 11:53 AM | |
Joined: 10/11/2006 Last visit: 4/26/2024 Posts: 5824 Rating: (789)
|
Hello, there are tests planned about the technical feasibility to connect 690V PM240-2 on a chassis BLM/SLM, but the tests are still outstanding. So at the moment the DC bus coupling of PM240-2 on a SLM is not released. In connection with the latest firmware version 4.8 the PM240-2 could be used with a CUA32 on a CU320-2. https://support.industry.siemens.com/cs/ww/en/view/109740192 You have to consider some compatibility fact regarding the hardware version, then it will work. https://support.industry.siemens.com/cs/ww/en/view/109737902 You can find all the supported Power Modules in chapter 4.2 of the actual AC Drive device manual. https://support.industry.siemens.com/cs/ww/en/view/109740027 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on