Industry Online Support
Technical Forum
6/21/2014 9:10 AM | |
Posts: 3 Rating:
|
Hi, I have above hardwares; - Sinamics S120 (CU310-2DP and PM340 power unit) - 1FK7083-2AF71-1RA0 motor - MPI/USB cable I can connect the driver via MPI/USB cable in STARTER. I properly did the configuration of driver according to power unit and motor. Motor turns well when i choose "Positining Mode - Basic positioner - Positionin Relative". However when i choose "Positioning Mode - Basic Positioner - Positioning Absolute". motor does not turn and a message appears at alarm window. Message : 7461 : EPOS: Reference point not set. I attached related pictures. How can achieve this problem? Thanks. AttachmentAbsolute Alarm Relative.pdf (247 Downloads) |
6/24/2014 2:36 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 177 Rating:
|
New question split intoSINAMIICS drive - Where can set establish a"zero" point. With best regards, Narrator1
|
This contribution was helpful to
1 thankful Users |
6/24/2014 2:59 PM | |
Joined: 5/23/2011 Last visit: 12/1/2022 Posts: 3 Rating:
|
Please go through attachment there is eample of S7-300 & S120 communication through profibus in positioning mode with detail explanations.
AttachmentEz_epos.zip (443 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on