10/26/2015 2:00 PM | |
Posts: 2 Rating:
|
Dear All, I have a problem regarding a S120 application I'm working on. The problem is that " There is Atlas machine our rewinder arm used drive is S120, Motor and encoder power given through male and female socket, our machine running ok but some time stop due to fault code 7901, after this we reset fault and its acknowledged and machine start, I check all cable its ok encoder is also working ok but again facing with same problem by 10-12 hours or a day my issue is that can we bypass this fault or can we increase the time of sensing of over speed please give me suggestion, can i change perameter for positive rotation P1085&P2162, and for negative rotation P1082&1088 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/27/2015 11:02:29 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
Follow us on