11/2/2020 1:00 PM | |
Joined: 9/23/2005 Last visit: 2/1/2023 Posts: 4087 Rating:
|
Check in the List manual what is the acknowledgment strategy for the fault you get. I.e. if it is not POWER ON. |
Regards, |
|
11/2/2020 1:56 PM | |
Joined: 7/11/2019 Last visit: 1/9/2023 Posts: 31 Rating:
|
Yes, I understand what you mean, I know there are an errors, which want restart (POWER ON) of machine, but this is not exactly answer for my question. My question is, what way of acknowledgement is recomennded for me. a) Laxisctrl reset? b) Laxisctrl reset with restart? c) DPWR_DAT with rised bit which targets to r2090.0? <- Here I do not know, if this is controlled by laxis ctrl or something else and if I am autorized to legally acknowledge it by DPWR_DAT d) or something what I do not know? There is also a "Diagnostic" menu in TIA with "Alarm display" and inside is "Acknowledge" button. Which help me lot. How can I control this ack procedure? Imagine a machine which works well for now, but when an error occurs, I am not able to resolve it without TIA portal. I want to have a global acknowledgement button in HMI for errors which are acknowledgeable. But I do not know how to akcnowledge it from PLC (I am not so advanced user). Thanks for help. |
11/3/2020 4:08 PM | |
Joined: 10/11/2006 Last visit: 2/1/2023 Posts: 5410 Rating:
|
Hello, Control Unit faults cannot be acknowledged via TO-Reset / TO-Restart. The LAxisCtrl TO-Reset will only acknowledge the corresponding Drive Object of the SINAMICS. Recommendation:
|
With best regards, |
|
This contribution was helpful to
3 thankful Users |
11/19/2020 5:37 PM | |
Joined: 7/11/2019 Last visit: 1/9/2023 Posts: 31 Rating:
|
Using of Sina_Para_S is easier than I thought - this is the way for me, thank you. But, I do not know how to exactly handle this:
As begginner, I do not know how to handle telegram 39x (in diff way than DPWR_DAT / DPRD_DAT). In tags I have only deffined telegrams 105 for axes, but 394 telegram is not defined. Telegrams 105 was created automatically with TO (I think). Funny is, that I do not know where appeared I262.0, Q262.0 (and else in attachment). I know, when I have some I and Q, they have their address in Device view. Maybe I understood it wrong. Anyway Sina_Para_S is solution. Thank you. |
Follow us on