Industry Online Support
Technical Forum
12/19/2014 6:48 AM | |
Joined: 5/12/2006 Last visit: 1/31/2023 Posts: 21206 Rating:
|
Hi, the used infeed is a 5 kW Smart line module without DRIVE-CLiQ interface, so you can't see this module in the Topology and not configure in STARTER. This type of Smartline you control with a DI/DO Interface, for correct wiring you should refer the Manual Capter 4.8. Regards Christoph |
This contribution was helpful to
1 thankful Users |
12/20/2014 2:28 PM | |
Joined: 1/30/2013 Last visit: 1/30/2023 Posts: 33 Rating:
|
Hi! One sentence: The best Forum ever ;) Thank YouChristophD. When I connected infeed module like inManualCapter 4.8 then everything started work! greetings! |
Last edited by: Aleksander EUTECH at: 12/20/2014 2:29 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on