3/31/2017 9:18 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, 1)When drive is completely shutdown (no power or control voltage) only your real multiturn of the encoder is relevant. When drive is powered off and you manually move it > than 1/2 multiturn (4096/2 = 2048) the drive has after power on again a false position. 2) With 'rotary axis' you can define a bigger range as with 'linear axis'. It is described in FH1. 7.22 Position tracking https://support.industry.siemens.com/cs/ww/en/view/109740020 Virtual multiturn encoder (p0412) With a rotary absolute encoder (p0404.1 = 1) with activated position tracking (p0411.0 = 1), p0412 can be used to enter a virtual multiturn resolution. This enables you to generate a virtual multiturn encoder value (r0483) from a singleturn encoder. It must be possible to display the virtual encoder range via r0483. Note If the gear factor is not equal to 1, then p0412 always refers to the motor side. The virtual resolution, which is required for the motor, is then used here. For rotary axes with modulo offset, the virtual multiturn resolution (p0412) is preset as p0421 and can be changed. For linear axes, the virtual multiturn resolution (p0412) is preset as p0421 and extended by 6 bits for multiturn information (max. overflows 31 positive/negative) If, as a result of extension of the multiturn information, the displayable area of r0483 (232bit) is exceeded, the fine resolution (p0419) must be reduced accordingly. |
With best regards, |
|
10/2/2017 10:27 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (40) |
Hello, Looked through my projects just out of interest, because this issue is acute for me as well. So I would say that 1/2 multiturn has nothing to do with this case. Also, see encoder logic homemade chart attached where you'll find an explanation. Msorich Attachmentencoder_logic_chart_003 Copy.pdf (540 Downloads) |
10/3/2017 9:55 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (40) |
Well. Does youre encoder have any name? Just out of interest to look at its technical data. Msorich |
10/3/2017 3:57 PM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating: (40) |
Well.What about 12 bit resolution encoder + 13 bit multiturn capacity? What happens in this case? Msorich |
Follow us on