6/30/2009 8:15 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi normally it is not adviced to connect two motor to the same brake terminals, i have attached some documents which gives you information about the BR+ and BR- with regards ram Attachmentbrake.pdf (715 Downloads) |
7/1/2009 3:45 PM | |
Joined: 9/18/2006 Last visit: 2/6/2024 Posts: 589 Rating: (64) |
Hi. Best regards. AttachmentMotor changeover.pdf (477 Downloads) |
11/12/2009 11:41 PM | |
Posts: 139 Rating: (25) |
You want to know how to control the BR+/- terminals then the easiset thing to do is for you to look in the list manual. Just setting the parameter P1215 is not enough you also need to configure how the brake will operate. From the screenshot you gave I can see that the brake is closed. I expect you are trying to open it? http://support.automation.siemens.com/WW/view/en/33974002 For you to understand what is happening you will need to look at function diagrams 2701, 2711, and 2814. |