12/17/2015 7:08 AM | |
Joined: 5/12/2006 Last visit: 6/6/2024 Posts: 22255 Rating: (2986)
|
Hello, which SW Versions do you use for Starter and Step7 ? Regards Christoph |
12/17/2015 8:12 AM | |
Joined: 5/12/2006 Last visit: 6/6/2024 Posts: 22255 Rating: (2986)
|
Hi, the prob is that in the STARTER Version V4.3 the SW DriceES Basic is needed for a correct integration of the Starter devices in Step7. Have you a driveES installation on the System? If no then uninstall Starter V4.3 , Install the Step7 SP4 and after that install the latest Starter V4.4. The latest Starter you can download here: https://support.industry.siemens.com/cs/ww/en/view/26233208 This message with Reason 211 means that there a some internal data not ok, this can happens if the wrong SW Combination is use for configuring the System.
Christoph |
12/17/2015 10:16 AM | |
Posts: 7 Rating: (1) |
In the download link you've given to me the file name of the ZIP file only mentions G110 and G120 : Vol_1_STARTER_V44_SP1_Program_G110_G120.zip (1,2 GB) optionally: Vol_2_STARTER_V44_SP1_SSPs_Rest_of_SINAMICS_Family.zip(719,1 MB) optionally: Vol_3_STARTER_V44_SP1_HELPS.zip (1,0 GB) And while running the Setup, there was no option for S120 (I've downloaded and extracted these 3 zip files and launched the setup.exe from CD1). Maybe this is something that will come after or that I can download from somewhere else. |
12/17/2015 11:22 AM | |
Posts: 7 Rating: (1) |
Here is what I have with the new starter. I've also displayed the online FW versions if this might be of any help. Regards, Joël |