12/17/2015 10:16 AM | |
Posts: 7 Rating: (1) |
In the download link you've given to me the file name of the ZIP file only mentions G110 and G120 : Vol_1_STARTER_V44_SP1_Program_G110_G120.zip (1,2 GB) optionally: Vol_2_STARTER_V44_SP1_SSPs_Rest_of_SINAMICS_Family.zip(719,1 MB) optionally: Vol_3_STARTER_V44_SP1_HELPS.zip (1,0 GB) And while running the Setup, there was no option for S120 (I've downloaded and extracted these 3 zip files and launched the setup.exe from CD1). Maybe this is something that will come after or that I can download from somewhere else. |
12/17/2015 11:22 AM | |
Posts: 7 Rating: (1) |
Here is what I have with the new starter. I've also displayed the online FW versions if this might be of any help. Regards, Joël |
Follow us on