4/16/2018 10:46 AM | |
Joined: 10/11/2006 Last visit: 2/8/2023 Posts: 5418 Rating:
|
Hello, correct, you have to use one safety license per axis which is using extended functions. If no PROFIsafe should be used you have to use F-DIs for SLS selection. Therefore you can use a TM54F for the CU320-2 or the CU310-2 which comes with F-DIs onboard. You can find different connection methods connecting F-DIs to F-DOs on the following FAQ. https://support.industry.siemens.com/cs/ww/de/view/39700013/en |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
4/16/2018 4:16 PM | |
Joined: 9/17/2010 Last visit: 10/27/2022 Posts: 11 Rating:
|
OK, Now I have all answers. |
Follow us on