2/24/2018 7:39 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, if you use a SIMATIC / SIMOTION you can use the axis control block: https://support.industry.siemens.com/cs/ww/en/view/48816191 Or if you use the basic positioner you can use the traversing blocks with the functionality "traveling to fixed endstop". If you use only speed controlled axis, I would use telegram 2 with additional data´s, where I can send the torque limits (and connect the PZD´s to the torque limits). So when the torque limit is detected, the torque limit would be active. Zako |
This contribution was helpful to
1 thankful Users |
Follow us on