7/22/2013 7:30 AM | |
Posts: 251 Rating: (11) |
hello, do you have any document for it? i have cu310 pn and s7 1214 c cpu how can i add adress? best regards
|
7/23/2013 1:54 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, At the moment there is no standard application with S7-1200 and S120 available. But - you can have / use some inspiration with this topic: This example shows the important steps for a G120C - instead of this drive you can use also the CU310-2PN with GSDXML file. http://support.automation.siemens.com/WW/view/de/56749384 Another application is based on Startdrive: http://support.automation.siemens.com/WW/view/de/70155469-> the main diffrence is to skip the G120 content for Startdrive |
With best regards, |
|
Follow us on