1/27/2021 2:55 PM | |
Joined: 10/11/2006 Last visit: 2/3/2023 Posts: 5412 Rating:
|
Hello, this you can do only applicative. Use a bero to detect home position, and use it as measuring input. 4.1.2 Configuration - Hardware interface (S7-1500, S7-1500T) Using PROFIdrive telegram of the drive axis: • SINAMICS S210 (X130 "MC_MeasuringInput" (Onetimemeasuring) https://support.industry.siemens.com/cs/ww/en/view/109766466 Use the measured value to calculate "home position" for "absolute encoder adjustment": MC_Home command with mode 6 or 7 |
With best regards, |
|
This contribution was helpful to
3 thankful Users |
Follow us on