Industry Online Support
Technical Forum
5/11/2009 3:23 PM | |
Joined: 3/21/2006 Last visit: 12/4/2023 Posts: 10222 Rating:
|
Hello, You didn't said anything about other existing hardware in S5-115U system. And I assumed you will use AS511 port from CPU to establishe connection. In WinCC, there are communication drivers available in order to establish a serial communication link to the SIMATIC S5 family. • SIMATIC S5 PROGRAMMERS PORT AS511 Communication using programming interface of the respective CPU. Be carefull for each COM port of the WinCC station, a maximum of one PLC is accessible. So, how to configuring communication to S5 look at http://support.automation.siemens.com/WW/view/en/22779871 Hope this will helps. Best regards Hristo Mihalev |
Follow us on